APC3200: RAM expansion via the second slot?

Hi everyone,

I currently have an Automation PC 3200 (APC3200) equipped with 8 GB of RAM.

I would like to know if it’s possible to expand the memory by using the second slot—for example, by adding another 8 GB stick to reach a total of 16 GB.

Does the hardware support this specific configuration, and are there any specific technical requirements I should be aware of?

Thanks in advance for your help!

Yes it is possible to install more RAM to the APC3200(and PPC3200), instructions available in Automation Help here:
Installing the interface option and DDR4 SDRAM

With RAM you should keep in mind that the two RAM sticks must have the same speed and timings, preferably they should be identical, to ensure best performance & stability.

You may inquire your B&R contact for additional RAM as these are also available separately from B&R.