How can i download backup program to 3ip350 b&r cpu? have pg2000 and establish connection ..no knowledge of using pg2000
Hi Sardasai,
With SYSTEM 2005 controllers or with the newest ones, the answer is the same as Wenbo answered in another similar question.
Xabier,
Thank you for response. I have backup of the source code for “ip350”,in the file extension .pgp.
How can i get this file to download using pg2000 ( dos based B&R). to the I350 processor?
Regards
Hi Sardasai,
Please check manual of the SYSTEM 2005.
System 2005 User´s Manual | B&R Industrial Automation (br-automation.com)
Those PLCs were already programmed using Automation Studio. If you have the project with extension .pgd then it was developed using Automation Studio 2. On our website you can download it.
Automation Studio V2.7 | B&R Industrial Automation (br-automation.com)
Take into account the support OS of it: WinXP, Win7/32bit
You can connect via serie to the IP350 and download the project.
Be careful with these material, it is really old and it has been already discontinued to buy and repair. Also the support to those old material is really limited.
If you have more doubts, please contact to your local B&R office.
Locations | B&R Industrial Automation (br-automation.com)