BnR Automation Studio Installation 4.12

Hi,

I had the same problem or better the same windows error message.

Immagine che contiene testo, schermata, Carattere  Il contenuto generato dall'IA potrebbe non essere corretto.

I was trying t install the upgrade inside AS4.12.6 un upgrade, but in the B&R Sites the was the documentation to install outside the AS. Both for the 4.12.7 or for the 4.12.8.

So the solution is to follow the B&R documentation.
Installation_of_Automation_Studio_Version_4.12.7_English.pdf

Installation_of_Automation_Studio_Version_4.12.8_English.pdf

1 Automation Studio 4.12.8

1.1 installation

Run the executable file Automation Studio.exe from the installation directory above the

already installed Automation Studio 4.12.6.

Please use the B&R Automation Studio upgrade dialog if AS 4.12.7 is already installed

I usually install using the upgrade tool inside AS , I don’t often look at the download section of the site of B&R; but there is a link to show this different procudere.

Immagine che contiene testo, schermata, Carattere, numero  Il contenuto generato dall'IA potrebbe non essere corretto.

1 Like