Upgrade services does not work

Hello comunity,
When i try to install the upgrades, it comes out this window:

Also during the installation of Automation Studio it comes out a pop-up that says that the Upgrade service doesn’t manage to start(and I think that is linked with the previous problem).

So basecally the problem is how can I start manually the “B&R Upgrades Service” to install the Upgrades?

Information of the installation:
-Automation studio version: 4.12
-System: Windows 11 (64 bit)

Thank you

Hello Alessandro, welcome to the B&R Community!

Not sure why the service wouldn’t start automatically but you can check your Task Manager under Services. If the service for AS412 is not started try starting it manually.

Thanks for the answer.
But when i try to start the service manually, there is an authorization error (error 5):

In the pop up there is written : “Impossible starting B&R Upgrade service for AS412 on local Computer. Error 5 Denied access”

Basecally, it seems that is a problem of authorization, so how can I solve this?

Thanks

Hi,

it seems that your current active Windows user does not have the right to change service settings, the error message “error 5 access denied” is directly thrown by Windows.
Does your Windows user have local admin rights?

Best regards!

Hello,
I have managed to solve the problem, Thanks for the suggestion.

Best regards

Would it be possible to share the solution you found? This may help someone else in the future!

Basically, I went in the properties of the service (right click in B&R upgrade service of the previous photo). And here I enabled the comunication with the desktop (because I have the installation file in the desktop)


And after these the US have started working

Quick Info for others on how to open the Windows-Services:
Win+R >> type “services.msc” >> Enter

Is there a way to install the upgrade service for AS 4.9 ? I had to reinstall AS and now i cannot use the update option.
image

The upgrade service should be installed when AS is installed. If it’s not available in your Services list, then something didn’t install correctly and I recommend reinstalling Automation Studio.

I’ve tried creating my own upgrade service before and the result was not pretty :sweat_smile:

Here is an alternative method using PowerShell.

  • Open PowerShell with Admin rights.
  • Input the following to get a list of B&R Upgrade Services
    Get-Service | Where-Object {$_.Name -like "*BrUpgrSrv*"}
  • Then run the following command to start the one that best fits your version of Automation Studio. The following example is for Automation Studio 4.12.
    NET START BrUpgrSrvAS412

Thank you for sharing. I had the same problem when after installing AS 4.11 on Win 11. Also had to enable .net 3.5 feature.

This solved my problem for me as well. Pretty useful !