Connection to an ACOPOS 1022 via an X20 CP1583

Hi @Luis_Finke ,
Can you login on our website?
If yes please download this training module:

TM410 – Working with Integrated Motion Control

In the module at this page you see basic command power/home/move velocity/stop:

At the page 31, you see some information about our system diagnostics manager tool, there is section focus on the axis:

You have CAN card interface 8AC110.60-2, not supported in mapp Motion:

At this point continue to work on your configuration with ACP10 axis control, and please don’t try to configure the prj with mapp Motion.
When you are ready to control your motor inside your program, I recommend to use these couple of Function blocks:

Ciao
Valerio