After transfer new OS 2.51 (switch in position 0) can’t go to online mode to transfer project (switch in position 1) I’m using AS 2.7.0. COM1, 115200, none - nullmodem (I used other speeds without result - tools-> option → Online → Online configuration). I’m trying configure Acopos 8V1022.00-1 and only AS2 support this CPU and Acopos.
look at this @Pawel_Zwolak …hehe
but for 8VI1022-1 is different story, we need CAN interface and old motion library no more supported on AS 3 and 4
==========
What do you see for status indicators?
=========
If you manually change the operating mode to “Boot” can you connect to the system?
Ciao
Valerio
ERR and RDY → lit. RS232 → flickering one per sec. If I change to “0” I can transfer OS to PLC, but after succesfull transfer can’t connect in “0”, “1”, “F”.
Please check the serial interface settings in the project and adjust the online connection settings accordingly.
Hi @Pawel_Zwolak , can you share with us what is status of your issue and final conclusion, if possible mark a solution and Help Us Keep the Community Organized