Default Login for X67 module

We recently received an ABB robot that has a few B&R modules installed. One of the modules has quit responding and I was attempting to connect with the web interface.
I am unable to see any of the parameters. I see it is requesting a username and password.

Is there a default username & password for the X67?

Thanks for your help,

Dennis Fairchild

Hi Dennis,

Do you know which B&R modules are on your machine? X67 is a series of IP67 rated I/O modules that are designed to be mounted outside of a cabinet. They aren’t something you would log in to. The one exception I can think of off the top of my head is the EtherNet/IP Bus Controller module. This is used to connect B&R I/O to a 3rd party EtherNet/IP Master (i.e., the ABB robot controller). This has a web interface which lets you configure the communication, but I’m not sure if this would help you. The default username and password for that are in the EtherNet/IP Bus Controller User’s Manual:

Does the machine have a B&R controller (PC or PLC)? There are some additional tools available in that case.

Marcus,

Ours is the Ethernet IP model X67BCD321.L12.

It is connected an ABB Robot controller. I was trying to open the web interface so I could look at the configuration of the module.

I’ll try the username / password you recommended.

Thanks for your help.

Dennis