Hello,
I am coming back to you with a structured customer request regarding hoist/winch cable tension control, based on concrete field feedback.
Current situation
The customer is already estimating the load via the drive sing the following principles:
Reading of magnetizing current / effective motor current
Motor torque calculation
Indirect estimation of cable tension
The theoretical fundamentals are therefore well understood by the customer.
However, they are facing significant limitations in terms of accuracy and repeatability, mainly due to:
Strong variations of mechanical efficiency over time, major influence of the number of cable layers on the drum** (hoisting vs lowering completely changes the real load), temperature effects, overall, mechanical losses (gearbox, drum, cable guidance).
As a result, the torque-based estimation at motor level is often **far from the real cable tension.
In parallel, the customer does have **advanced solutions with dedicated load sensors, but these are considered:
costly,
complex to integrate,
poorly suited for certain **special-purpose machines (perceived as “overengineered” solutions).
Questions to B&R
In this context, could you please clarify:
Does B&R offer a tension control or regulation function integrated in the ACOPOS drive, beyond a simple motor torque estimation?
If yes:
on which physical and algorithmic principles is it based ?
what are the known limitations with respect to the phenomena mentioned above (cable layers, mechanical losses, temperature, varying efficiency) ?
While I can’t confidently say that B&R has an immediate solution for this case scenario, I think a look at “mapp Web” or the “Winder Closed-loop tension control” example might be something check out. Maybe someone might be able to dive deeper into the “nitty gritty” of things.
i am not an expert for hoisting or winding and the issues you descripe that the motor does not see the direct load due to mechanics is often an issue you can only solve with a sensor.
But for your question about how the Torque is calculated i think this article in the Automation Studio can bring you a bit forward. There are different possible modes descriped. Mainly a Default-Mode and a Advance-Observer Mode.
Hi @kovarj At this stage, I haven’t received any concrete progress. Apart from the two feedback points mentioned earlier, there has been no additional response.
I shared this feedback with the customer, but so far it hasn’t led to further advancement on the topic. I will keep you informed as soon as I receive any new updates.