I have a big problem on all of my as versions that are installed ( 4.2 - 4.3 -4.9 4.12), i cannot find any PLC connected to my computer,
When my plc have an IP number that was assigned before the problems started, i can download the software but when a want to assing an IP number to a new plc i cannot find the device.
i’ve tried to reinstall as 4.12 ,
I’ve reinstalled pvi manager with the latest version
New PLC do not have an IP adress ( x20cp0411 and x20CP0484 ) allready programmed plc i can see them in run mode but they do not appear in the browsing screen
which AS 4.12 are you using? I see we have an issue: ’ Browse for targets never finishes and no SNMP response is received’ fixed in the version 4.12.11.2 SP:
I understand this is frustrating, but when you report an AS issue, we do need to verify that your specific AS version is supported by your PC’s operating system:
not sure if it helps, but: as far as I remember, the PVI4 snmp functions use the WinPCap driver for low level network packet inspection.
If that driver is damaged or updated from another software to a incompatible version, I could imagine that snmp does not work anymore.
So I would sugest to
check in the extracted PVI setup if you find a setup named winpcap
execute just this setup
if asked for “deinstall installed version”, confirm and deinstall it
restart and try again
I’m not at PC right now, so I can’t give more conrete advice.
But maybe it’s worth a try?