Respaldo de PLC X20 BC 0083

What kind of PLC is connected to the X20BC0083? If the PLC has a removable memory card, you can use Runtime Utility Center (included in the installation package for Automation Studio). See this post for some helpful screenshots.

A couple of things to keep in mind:

  • This is a 1:1 backup and so must be restored on the same memory card (or a card of the same size)
  • Without the source code (which is not stored on the PLC) you cannot change the program or hardware, which means you’ll have to put this card back into the same kind of PLC it came out of