Runtime directory Error when building solution

Hi community,

I did a downgrade of the AS version from 4.2.14 down to 4.2.10 and afterwards I got the following error when I try to build or rebuild the project:

Error 9225: Could not find Automation Runtime directory K4.26.

I have check if the directory is in the project folder and also, re-install Runtime k.26, but it doesn’t fix the issue.

Have some of you guys experienced such an issue?

Thanks in advance :slight_smile:

Regards,

Dioni

Hi again,

For the record, I found the solution to the problem. I reloaded and applied the runtime version (the same: k4.26) using the “Change Runtime Versions” tool.

Then the project compiled normally without the error described in the previous post.

Dioni