Welche AS Software bei AC1045.00-1 | Which AS software is used with AC1045.00-1?

Hi @Maxi
Feedback from Support:

”When the customer has a machine which is using a combination of AC112 and AC114 then they need to use PLK V1 and need to stay on ACP10 V2.xx.x versions otherwise AC112 won’t work anymore. The latest version in the ACP10 V2.xx.x family is V2.52.8 indeed. This is “so far” away from V3.xx.x because we simply made a version jump with ACOPOS P3 to V3.xx.x Similar to the jump we made from ACP10 V3.18.2 to V5.xx.x and the jump we are going to make from V5.27.x to V6.xx.x”

Versions:

Powerlink V1:

Ciao
Valerio