Why does mappView fail to open after SSL setup

I tried the mentioned settings - In addition to that i also made settings in the webserver setting of PLC and added SSL configuration there. After that the satefy msg was gone. But then i get this error and mappview does not open.

What can be done next to resolve this “Error in configuration”?

Hello,

Which port have you configured for the mapp View? Isn’t there a collision with the Web Server port number?

What is the full address you’ve added to the address bar? If https is there as the protocol and since there is no port number specified, I guess it defaults to 443.

Hi @Sharmah ,what is status of your topic? can you provide info Pavel asked you for?

After the sugets from Pavel - i changed the websrever port.
Then it worked, as he mentioned - Mappview and webserver were assigned same port - may be that was the issue.

How ever now it works.

Thanks B&R community

Can you mark Pavel’s answer as the solution? That way, the thread is closed, and others can see what the solution was for you.