X20ds4389+ x20bc0087

Dear all,

i’m tring to use the X20DS4389 (time stamp) + X20BC0087 (Modbus).

i use the Automation studio to create ModbusConfig.xml file and i program it via ModbusTCP Toolbox.

all look ok, but i get no actual register from the X20DS4389

i also red on the net you need to set the function model in the configuration of the X20DS4389 to Function Model 0 or 1 but i can only choose Default, why is that?

below is a screenshout of the configuration of the X20DS4389

to summary my questions -

  1. why i see in the X20DS4389 configuration function model only Default?
  2. is there V6.0 HW Upgrade (X20DS4389) available?
  3. any other help will be appriciated.

thank you.

Hello Hadar,

the nettime function of the X20DS4389 is not supported on the X20BC0087.

Regards

Stephan

To get the timestamp of a “Edge” you need to configure this. Then you could do some basic calculations

Hi @HadarMagali what is status of your topic, can you update us and close this topic?

Closed by moderator.