Hi, I have an issue with two X20 modules, X20IF10E3-1.
In the Siemens Hardware configuration I have configured 6 times 64bytes in, and 32 bytes out, as I was told to by the supplier.
We use the latest GSD file, version 2.34.
Communication is established, but it gives an error telling us that slot 0 has an incorrect submodule. There is nothing else to choose in the catalog so I don’t understand what the problem is.
Does anybody now?
The top part in the screenshot below (with the slots) is from the supplier (not the Siemens configuration), the rest is online view on the Siemens side.
looking at your screenshot I see that on the B&R side the IF10E3-1 is called “NetX100”
This indicates a really old version of this card or to be more precise of the used firmware/hardware upgrade used inside Automation Studio for this card.
If I enter such a card within my Automation Studio it is correctly called “IF10E3-1” as you can see:
I will contact the vendor with this information since I am not familiar with or responsible for the X20 module and Automation studio. I only deal with the Siemens (PCS 7) side.
Will let you know the result once tried.
Thank you for the manual. Makes me understand better how the other party sets up the configuration.
Yes, I have added 6 times 64 byte input, and 1 time 32 byte output as submodules.
Not in TIA but in Step 7 HW config (since it is PCS 7).
I am just wondering now if their screenshot was supposed to be what we should configure at the controller (as I was told to do) or if it is how they configured the X20 device.
In that case, should the controller side not be the opposite, 6X64 bytes out, and 1x32bytes input?
I see we also have to make sure that we (still) have the correct device names of the two units when the vendor makes changes in the configuration (chapter 5.1.2.1 of this manual).
The modules are always seen from the master perspective, so if they define 64 bytes Input, you do the same. In AS they will show up as outputs. The important part is that they match exactly in size and that the device name is correct.
The screenshot with the “NetX 100” information was old. The device has the latest firmware loaded into it, v4.0
I got this screenshot from Automation Studio:
I don’t know what to make of that. How does this correspond to the (expected?) firmware V3.13 that I see in my Siemens hardware configuration coming from GSD v2.34?
What to do next? Supplier says their side works when tested against a testing system (no idea what system or software is used for that but I guess not a Siemens PLC).
Can anyone help there? @Noach, if you do not get an answer here, please get in contact with local support and share the link to this discussion with them. Thanks.
Hi Noach,
the firmware is fine. The readme gives you more details what module to use
GSDML file GSDML-V2.34-BuR-X20IF10E3_1-20191216.xml contains three devices (DAP´s).
"X20IF10E3-1_NETX V1.0.0.0-V1.2.x.x" Shall be used for Automation Studio HW upgrades with versions from V1.0.0.0 to V1.2.x.x (no PNO certification).
"X20IF10E3-1_NETX V1.3.x.x" Shall be used for Automation Studio HW upgrades with version V1.3.x.x or higher (PNO certified with Automation Studio HW upgrade 1.6.0.0).
"X20IF10E3-1_SAFE_NETX V1.3.x.x" Shall be used for Automation Studio HW upgrades with version V1.5.0.0 or higher in combination with the openSAFETY gateway X20SL8110 (PNO certified with Automation Studio HW upgrade 1.5.0.0).
For up to date projects you always use “X20IF10E3-1_NETX V1.3.x.x”. Delete the IF card form AS and add it again. Configure 64 bytes input and 64 bytes output for testing purpose. Leave everything else as it is. Follow the guide to configure the Siemens side.
If that still does not work post some screenshots what error messages the Siemen side shows.