Just a general idea of where to start: if you are not sure if the hardware (HW) state is correct, please use the system diagnostic manager to check the status of your complete HW configuration. Additionally, the logger can provide you with a basic overview of possible problems.
you can also use conversational help. B&R Online Help and ask for some hints, this can also help. Please we aware that AI generated answer can be wrong
so basic technical user knowledge is needed ![]()
Hi,
I would check first the led status of the X67 module. It could be a wrong wiring.
As @kovarj said check the SDM for maybe other module error and the logger for details informations.
Hello,
The Error Code 6057 can be checked in AS-Help. (see Picture)
It indicates an Error on the Encoder connected to the Axis.
Based on the fact that your Screenshots and Ordernumber advise that it is a Steppermodule you are diagnosing. You may check this diagram for wireing.
The module normaly indicates this error via EncOk01 for Axis 1 and EncOk02 for Axis 2
You did indicate that you do not have the software running on the plc (in another thread). This limits the possibilitys drasticaly as you would not be able to make a transfer of changed settings. You have to trust that the program and settings on the plc are correct to drive the motor.
Greetings
Michael
Is it possible that this error is caused by the wrong version of the X67SM2436 module (which I use for the stepper motor)? I mean, there is not only a part number on the module, but also a version number (e.g. ver. H0, ver. P9). I am not on the site right now and do not remember the version. However, could this be the problem?
Hello,
The Revision Number (e.g. ver. H0, ver. P9) is used to mark different Hardware implementations of the Module (eg. change of a Resistor supplier). If the module has the same Productnumber it is meant to be compatible without restrictions. But in very rare edge cases a different Revision can cause issues, for example if the application was slightly out side of spec and was only lucky to work with a special Revision, but with an other one it doesn’t.
If a module as known compatibility issues B&R adds a -1 to the Productnumber to alter the number and symbolise the limited incombatibility.
The Revision can be read via SDM if a remote connection is available.
http://<IP-PLC>/sdm/hardware.html
It is possible but not intended.
If you have multiple Modules in the Machine a switch between a working and not working one would give additional information about this topic.
Greetings
Michael
Unfortunately, didn’t…
IIf it works out, let me know. And the same will happen from my side.
Hello,
as this seems to be a hard to diagnose error from the distance and the documentation about the error number hinting to the encoder did not help you. You could get in contact with a local B&R support and disscuss possible further options.
Also contacting the machine manufacturer would be a idea. As we can now see that more than one machine of this manufacturer is having the issue.
Sorry that i can’t provide you more ideas from the distance.
Feel free to continue the discussion here.
Greetings
Michael
Agree with Michael, please get in contact with you local support office. Please update us with possible solution. Thanks
The problem was with X67SM2436 and encoder (I suppose it was noise in power bus). I didn’t find out solution so just replace X67SM2436 to module of another vendor and connect it through CAN bus (it was on site already)