Firmware update request for PPT50.101E-16A

Automatic translation:
My 6PPT50.101E-16A control screen has recently had two issues: one screen frequently crashes, but the screen is normal (no touch response), and every time the power is restarted, it returns to normal. However, after about two days, the screen freezes again. I checked the firmware version 1.5; please see the pictures. I wondered if upgrading to the latest 1.8 firmware would improve this issue. Another screen has contact drift because this screen cannot be manually calibrated at 5 points, so there is currently no solution. I wonder if anyone else has encountered similar issues. Could you please share your valuable advice and experience? Thank you

touch drift

Can be caused by:

  • touch layer aging/damage,
  • mechanical stress/mounting pressure,
  • grounding/noise issue

Especially mounting pressure can happen if installation is not done according to manual. Usually sending to repair department is the only option. But for sure you can try to update and do electrical check..etc

About the freeze

  • Firmware updates often include stability fixes, so 1.8 is worth trying.

After update, record:

  • freeze interval,
  • CPU/memory trend,
  • ambient temperature

Especially memory trend recording can be interesting to exclude possibility that freezing is not caused by memory leak.

Yes, only the touch points at the very top and bottom of the screen have drifted. Be careful to touch other areas to ensure the actual position is affected. The same issue persists even after replacing the control screen with a new touch panel. Thank you for your reply!

Thank you for your reply. I will go and upgrade the firmware version 1.8 to review the several key points you mentioned. I will share with you in a timely manner if there are any good results.

Download 1.8.1.0 (AS6_PPT_50_v1.8.1.zip) via USB flash drive for upgrade

This is the HMI system information currently in use on site

HI @wanghaining , just tip for you. Do you know that you can write post in your language and use AI function for translation? If you use that function, more people will react to your questions :slight_smile:

If you have problem with new panel as well, then is really important to do EMC check. I would say, try panel in your office, on the desk where you can be sure that there is no problem with electrical disturbance etc.

Yes, this feature exists, but it always crashes when I use it, so I stopped using it. Next time I’ll translate to English before posting for help.

maybe you can send me short video, what do you mean by “crashes when use it”? I have not had reported any issue with using this feature.

I’ll give it a try, and I find it’s working again.

Hi @wanghaining , what is status of your issue, can you update us and Help Us Keep the Community Organized?