Hello everybody,
I want to upgrade my X20BC0087 Modbus TCP Bus Controller. In the manual it is stated that there are different versions.
I know how to make it (Modbus TCP Toolbox).
See also here:
Using the web server works for newer EtherNet/IP bus controller modules. However, older firmware versions are not compatible with modern web browsers. The classic error signature is that the web page loads, but no values are populated.
[image]
If you do not have access to an old Internet Explorer browser, then you can use the following workaround through the ModbusTCP toolbox.
Alternative Method using ModbusTCP Toolbox:
Download the X20BC0088 firmware and extract the .zip file (link bel…
But where to I get the newest Firmware, as it is not linked here:
https://www.br-automation.com/de-de/produkte/x20bc0087/#downloads
For example: for the X20bc0088, X20BC008U and X20BC008T it can be downloaded at their “Product-Page”.
So is there a hidden place where to find (e.g. Automation Sudio)?
Thank you for your help!
BR Gerhard
oliver_D
(Oliver D)
May 12, 2025, 4:45am
2
Hello,
firmware for non B&R fieldbusses is not available on the homepage nor in a “hidden” AS folder
It is only possibole to aquire this firmware via support
Please contact your responsible support office as they will provide you this firmware
best regards
Oliver