Cyril
(Giraudeau)
November 10, 2026, 4:28pm
1
Hi,
My customer is unable to compile his project when he inserts the module X20IF10E3-1.
He is running AS4.12.11 on a VM and I can compile his project on my side.
I suspect a problem with the DTM installation, so we did exactly this procedure : The DTM for '5ACPCI_XPNM_00' was not found - #4 by oliver_D
But the problem was not resolved.
As anyone an idea ?
Thanks
Cyril
Hi @Cyril ,
I did a small test and I got this error:
In my pc I have installed:
I closed AS and followed the instructions reported by Oliver, then I created a new AS prj and now no more issue with X20IF10E3-1:
Last note for the versions:
I don’t see anymore ‘B&R Generic HART DTM Release 5.2’
================
Try to create a new prj with just X20 CPU and X20IF10E3-1, should be ok.
As described by Oliver and recommend by Stephan:
=================
I recommend this post too: DTM Troubleshooting Guide - Share Info & Ideas / How-To & Wikis - B&R Community
Ciao
Valerio
HerbigS
(HerbigS)
November 10, 2026, 5:37pm
3
Hello Cyril,
I suggest deleting the Interface Card X20IF10E3-1 from the project and reinserting it.
Gruß
Stephan
Stephan, welcome (back) to the Community